------------------------------------------------------------------ File: Readme.txt Version: V1.1 Date: 14.02.2008 Description: B&R Windows CE5.0 PP300/400 ------------------------------------------------------------------ As follow you will find a short description and information to the version of the delivered software. ------------------------------------------------------------------ GENERAL ------------------------------------------------------------------ ------------------------------------------------------------------ Version V1.1 / 14.02.2008 / KEP ------------------------------------------------------------------ Changes - B&R Key Extension V1.0 added - Automation Device V1.21 added - Registry Editor V3.1 added - Windows CE 5.0 Update 070823_KB940981 added - Control Panel Applet "Touch Screen" V3.5 added - ELO touchscreen driver V1.16 added - B&R Set Date & Time V1.3 added - A driver for serial aPCI modules added - B&R Process Monitor V1.0 added ID 161980: VNC Viewer 3.6.2 added ID 145435: Touchscreen right click Error corrections ID 158845: Cannot set brightness and contrast of the display ID 162325: SSBlank uses up to 90% of the processor power. ID 167425: The applet "Terminal Server Client Licenses" can't be used on a QVGA display. ID 159725: Screen Rotate Bug. ID 161985: The PhysicalPageSize of USB stack has to be increased ID 160360: Internet Explorer doesn't download PDF files ID 174210: The touchscreen driver does not work correctly if the screen is rotated ID 152370: Empty string in SETTINGS.REG crashes the system ------------------------------------------------------------------ Version V1.00 / 30.01.2007 / KEP ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------